This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14020: Various characteristics over a limited temperature range

Part Number: LMR14020


Hi team,

Our customers are planning to use LMR14020 for a limited temperature range.

The limited temperature range is from -30 to 60 degrees.

Is there data that can tell the trend of Ven, Vfb, Ilim variation in this temperature range?

We are not seeking guarantee values.

If each parameter depends on temperature, we think that the variation range will be smaller than min or max in the datasheet.

If it depends strongly on the supply voltage, the range of variation will not change much with temperature.

Since they want to know the trend, they are most pleased if there is a temperature dependent graph of each parameter.

Please let me know if you have such information.

Best regards,

Tomoaki Yoshida