This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question of LED driver

Other Parts Discussed in Thread: LM3409, TPS54201, LM36011

We are looking for IC that meet the following conditions.

Please tell us the recommended products.

Vin=~12V

LED : 1ch and  1 LED

VF= 5V(max)

IC can set up the dimming timing by pulse from the outside.

(We want to light 1 mS out of 100 mS.)

IC can set up the IF from the outside.

(We want to set up 0mA~100mA while lighting.)

Does LM3409 meet the conditions?

Please let me know if there are other good products besides LM3409.

Best regards,

Takahiro Nishizawa