This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5020: Inquiry about lm5020-1, -2

Part Number: LM5020

Hi

My customer is developing an adapter with the LM5020.

The existing specifications are as follows.
Input AC 20 ~ 34V / Output 13V / 2A

However, the input conditions have been changed as follows.
Change specification
Input AC 20 ~ 34V / Input DC 21.6 ~ 26.4V / Output 13V / 2A

When LOAD is over 1.5A under DC 21.6V input condition
There is a problem that the output voltage drops after the duty is 50% limit.

LM5020MM-1 (Duty 80%) Can ic solve the above problem?
In general, we know that the duty is 50% in the FLYBACK circuit. Is it applicable to 80%?

The difference between -1 and -2 is the duty cycle limit, Slope Compensation, when I look up the datasheet. Anything else?
And can you explain Slope Compensation?