Having an issue with this.
Input battery power is set to 3.2V, the circuit beyond the bq25505 draws about 100 to 200mA (I can't find anything that says what the maximum output current of the bq25505 is)
Solar panel delivers about 5V (1Watt) panel.
There is a supercap to charge on vbatt_sec
The resistor setup is setup as below.....hope you can see this.
What we are running into a high frequency oscillation when vstore rises above 1.8V. It then cleans up when vstor gets to about 3.3V
VBAT_UV < VBAT_OV < 5.5V | VBAT_OV > VBAT_OK_HYST > VBAT_UV | 1.3V < VOUT < VBAT_OV | MPPT | ||||||||||||||||||||||||||||||||||
Desired | RSUM1 | 13 | MW | RSUM1 | 20 | MW | |||||||||||||||||||||||||||||||
Desired | RSUM1 | 13 | MW | VBAT_OK | 1.8 | V | > VBAT_UV | RSUM1 | 13 | MW | VIN_DC(OC) | 4 | V | Open Circuit Volts | |||||||||||||||||||||||
Desired | VBAT_OV | 3.8 | V | VBAT_OK_HYST | 2 | V | > VBAT_OK | VOUT | 1.3 | V | VREF_SAMP | 3.2 | V | MPP voltage | |||||||||||||||||||||||
closest 1% resistor1 | closest 1% resistor1 | ||||||||||||||||||||||||||||||||||||
closest 1% resistor1 | Exact | < | > | closest 1% resistor1 | Exact | < | > | ||||||||||||||||||||||||||||||
Computed | Exact | < | > | ROK1 | 7.865 | 7.680 | 7.870 | MW | Exact | < | > | ROC1 | 6.000 | 5.900 | 6.040 | MW | |||||||||||||||||||||
Computed | ROV1 | 6.209 | 6.190 | 6.340 | MW | ROK2 | 3.835 | 3.830 | 3.920 | MW | ROUT1 | 2.100 | 2.050 | 2.100 | MW | +10MEG2 | 10.000 | 10.000 | 10.000 | MW | |||||||||||||||||
Computed | ROV2 | 6.791 | 6.650 | 6.810 | MW | ROK3 | 1.300 | 1.270 | 1.300 | MW | +10MEG2 | 10.000 | 10.000 | 10.000 | MW | ROC2 | 4.000 | 3.920 | 4.020 | MW | |||||||||||||||||
Computed | VBAT_OV |
|
3.765 | 3.765 | V | VBAT_OK |
|
1.813 | 1.813 | V | ROUT2 | 0.900 | 0.887 | 0.909 | MW | +10MEG2 | 0.000 | 0.000 | 0.000 | MW | |||||||||||||||||
Computed | VBAT_OK_HYST | 2.014 | 2.013 | V | VOUT |
|
1.299 | 1.301 | V | VREF SAMP |
|
3.209 | 3.198 | V | |||||||||||||||||||||||
Selected | ROV1 | 6.34 | MW | ROK1 | 7.87 | MW | ROUT1 | 2.1 | MW | ROC1 | 6.04 | MW | |||||||||||||||||||||||||
Selected | ROV2 | 6.81 | MW | ROK2 | 3.92 | MW | '+10MEG2 | 10.00 | MW | +10MEG2 | 10.000 | MW | |||||||||||||||||||||||||
Selected |
|
ROK3 | 1.3 | MW | ROUT2 | 0.9 | MW | ROC2 | 4.02 | MW | |||||||||||||||||||||||||||
|
|
+10MEG2 | 0.000 | MW | |||||||||||||||||||||||||||||||||
Typ voltage3 | VBAT_OV(typ) | 3.765 | V | -0.94 | % diff | VBAT_OK (typ) | 1.813 | V | 0.70 | % diff | VOUT(typ) | 1.300 | 0.00 | % diff |
|
||||||||||||||||||||||
Typ voltage3 | VBAT_OK_HYST (typ) | 2.013 | V | 0.62 | % diff | VREF_SAMP | 3.198 | V | -0.05 | % diff | |||||||||||||||||||||||||||