This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS542951: TPS542951

Part Number: TPS542951
Other Parts Discussed in Thread: LM22676

Hello,

I'm a HW engineer for a Belgium firm active in the automotive business.
A couple of years ago i used the TPS542951 for one of my designs to generate 3.3 and 5V.
In the meantime we sold a couple of hundred devices which uses my board.
About 1-2% of the devices return with a smoked TPS542951. And i mean smoked. (see image).
The circuit was based on the one from the datasheet and integrated into the rest of the design.

My question is if there are other simular cases known and what the counter measures could be.