This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS549D22: Pin strap for RCSP bit field

Genius 17335 points
Part Number: TPS549D22

Hello

 

There is RCSP bit field in MFR_SPECIFIC_03 register.

Since Reset column of this bit field in the datasheet is “P”, it looks to be configured by pin strap.

But I can’t understand what pins are assigned to pin strap of this RCSP bit filed.

Could anybody tell me that?

 

Regards,

Oba

  • Hi Oba,
    Since this is a PMBUS part, the default programmed value for RCSP is R/1 [01b] and FS is 650kHz [011b]. You can only change these values via PMBUS and perform the "Store Config to NVM" which will allow you to reboot the part and maintained the last programmed value.
    Thanks,
    Amnat