This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: temperature for surrouding parts of LM25118

Part Number: LM25118

Dear Sir/Madam,

I used LM25118 in my design which output = 12V, 1.6A  and Input =10V to14V.

During operating condition, I found that the 2 Diode tmeperature is about 92 degree C,

2 MOSFET is about 82 degree C  and  10uH Choke Coil is about 76 degree C.

Part used for MOSFET :  Vds = 60V,  Id = 61A, Rds = 11.3m ohm.

Part used for Diode : VR = 40V,  IF = 5A

Part used for Coil :  Rated Current = 7.5A,  Rdc = 12.4m ohm.

Pls help to see whether I am using the surrounding parts which is lower in spec for this application.

Thanks.