This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C23: Feasibility Analysis

Part Number: TPSM846C23


Hi,

Please check the below specified requirement and let me know if this is possible with selected part which supports one time programmable feature along with VID programming.

 Requirements:

 Input Voltage: 11.4V to 12.6V

Output Voltage: 0.9V to 1.1V

Default Output Voltage: 1.025V

Output Current: 60A

Voltage resolution: 12.5mV or better

Regards,

Nitish