Other Parts Discussed in Thread: LM5023, UCC28730
Hi team,
Do we have a new Quazi resonant flyback controller like the UCC28600?
Parameters are as follows,
- Isolated
- Output Power - 24W
Thanks,
Needhu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Needhu,
LM5023 is very close to the electrical spec of the UCC28600. However, I am afraid we need more design spec to narrow down the best suitable controller.
Regards,
Sonal
Input voltage range, Output voltage, do they want to stick with Flyback topology? Why do they want a quasi-resonant controller, If Flyback is required can we interest them in UCC28730 which is also a Green mode controller with zero standby power.
Sonal