is it possible to have the LED come on immediately after the enable is pulled high? Because it takes a while for our SoC to boot, it takes ~30s for the I2C driver to come up and issue commands to the LP5562. However, we would like the LED to come on right as the board is powered. Is there some way to do that with the LP5562? Either with some kind of pull-up or pre-programming?