Other Parts Discussed in Thread: BQ25071, BQ25070
I am designing a single LiFePo4 cell charger from usb.
From the datasheet, BQ24079 have a VBAT target of 4.1V. Just wondering if anyone can tell me if LiFePo4 can handle this voltage? Most LiFePo4 datasheets will say 3.6 as the maximum voltage.
Also, with the dynamic power management (DPM) feature, does it mean that I do not need a separate USB detection circuit?
I have also looked at BQ25071, but it does not mention DPM at all, which is why i hope BQ24079 works out.
Cheers
Harry