Hello.
I have a question about UCC28070.
Data Sheet P35 8.2.2.8 Current Sense Offset and PWM Ramp for Improved Noise Immunity
, Recommended circuit for improving operation at light load (discontinuous operation) is described.
In addition to DC offset, triangle wave offset is added to this circuit.
Currently, we are checking the operation.
However, when operating with only DC offset, operation at light load is improved, but adding triangular wave offset lowers power factor and operation becomes unstable.
(In order to prevent erroneous current detection due to ringing when switching FET is OFF, I think whether only DC offset is sufficient.)
It is a question.
Adding a triangular wave offset lowers the power factor and makes the operation unstable.
What are the possible causes?
Is there a problem with handling only DC offset?
What is the reason for adding triangular wave offset?
Thank you.