Hi!
I planning to use the TPS5420 and I have a question regarding this IC.
Facts:
As voltage input I have a 230V/22V toroid transformer, and a Graetz-bridge rectifier. It means that my input voltage is 22V*sqrt(2)=31,1V peak.
Usually for the linear voltage regulators the circuit needs to have big capacitors after the brigde rectifier and before the regulator, to have a possibly constant voltage on the regulator input. However the TPS5420 datasheet ( I know it's DC-DC buck converter) says that it only needs 10uF filter capacitor on the input side ( even when the output is 2A).
Is this assumeing, that the input voltage is already constant? So do I need a bulk capacitor after my graezt brige rectifier? And how big( what are the calculations for it)?
This 10 uF filter capacitor should be (according to datasheet) a high quality ceramic X7R type capacitor and at least 35V type (beacause my input voltage = 31,1V), but rather 50V type. I have searched a lot and found that theese capacitors are really expensive if availably at all. Is it really that necessary? Or can I use a normal low ESR electrolyt capacitor? Are there any calculations on that, how the ESR of the input capacitor affects the circuit performance? What would be the consequence if a higher ESR capacitor was used? Blow up?
How big bulk capacitor do I need?
I also would like to run some simulations on this circuit, and for this I need some starting point. Is there a Simulink, Pspice, or any other simulation model available for this TPS5420?
Any books, links ideas are welcome.
Regards,
Miklos