This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: Output Noise and Switching frequency

Part Number: LM3478
Other Parts Discussed in Thread: LM3481

Hi, 

I'm designing a SEPIC based on the LM3478. Vin = 10 to 30V. Vout = 12V. Iout max = 700mA. SW Freq = 1M.

I've calculated all the values required for this features, but as you can see, when I connect a load for 100mA I obtain some spikes on the output and the switching freq is not the desired one (1MHz).

Have someone had this type of problems with the prototiping of this chip? What could I do or where could I start looking for an error?

Thank you.