This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: UCC28951-Q1

Part Number: UCC28951-Q1
Other Parts Discussed in Thread: UCC28950-Q1, UCC2895-Q1, UCC28951

Hello 

Can I use UCC28951-Q1 for larger input voltage range ( 310 Vdc to 410 Vdc ) for developing DC-DC converter ?

If not what is the range of input voltage for which this controller can be used ?

Is there any protection schemes such as Input and ouput over voltage , Input and output over current and under current ? please explain me.

  • Hello Rajasherkar,

    The UCC28951-Q1 can achieve a maximum duty cycle of 95%. These devices are generally fallowed by a PFC pre-regulator and have been designed for 300 V to 410 V input. With a maximum duty cycle of 95% you should be able to obtain and input range of 3:1 if you desired.

    You are correct that there are not input under or over voltage protection on these devices. I looked at the UCC28950-q1 and the UCC2895-Q1 devices and they don’t have this protection either.

    You could build an input under shutdown circuit with a differential comparator. The output would control a FET tied to the soft start pin. In the case of an under voltage keep soft start pin shorted to ground.

    I would recommend using this in peak current mode control, which gives you cycle by cycle peak current limit to prevent transformer saturation.

    Regards,

    Mike
  • Hello Sir

    Sorry , I forgot to mention that protection schemes to the dc dc converter not for the controller.

    Can I implement over voltage and under voltage protection to the both input and output sides of dc dc converter using UCC28951-Q1 ?

    In the same way Over current and under current protection to the both input and output sides using the same controller ?

    If yes , what will be circuit can i implement ? Please explain me.

  • Hello Rajashekar,

    The following link will get you to application note that shows how to use a hysteretic comparator. http://www.ti.com/lit/ug/tidu020a/tidu020a.pdf

    You can use the hysteretic comparator to drive a FET that can pull down on the soft start (SS) pin to disable the FET to turn of the gate driver when you desire.

    To both input under voltage and output over voltage your best bet is to use primary side regulation. This is where the UCC28951-Q1 would be on the primary.

    1. Input under voltage is the easy one. This would just require you to feed a resistor divider to the input of the comparator. This comparator would drive a FET and on an input under voltage condition would pull the SS pin of the UCC28951 low disabling the gate drive and reinitiating a soft start.

     

    1. For output over voltage could put the comparator on the secondary that could be FED into a logic isolator that drives a logic level FET that is connected to the SS pin of the UC28951. In the case of an over voltage will pull the SS pin low.

    Regards,

    Mike

  • Hello 

    sorry, I did not understand what you have mentioned earlier.

    In the figure no.55 & 56 of UCC28951-Q1 datasheet , Is there any over voltage and under voltage protection given in the input and output side of power circuit in the design of dc dc converter using UCC28951-Q1 ?

    if yes please explain the scheme given in that circuit.

    In the same way ,please explain the overcurrent and under current protection circuit in that design if employed ?

  • Hello Rajashekar,

    In the figure no.55 & 56 of UCC28951-Q1 datasheet , Is there any over voltage and under voltage protection given in the input and output side of power circuit in the design of dc dc converter using UCC28951-Q1 ?
    The UCC28951 does not have circuitry for input under voltage or output over voltage built in.
    The UCC28951 does not have under current protection.

    The design only has cycle by cycle peak current limit protection. The gate drive shuts down when
    1. The CS signal is greater than 2V refer to figure 36 in the data sheet.
    2. When setup in peak current mode control (Refer to block diagram on page 14)
    a. The CS signal and PWM ramp is summed and sent to the PWM comparator (PWM Comp).
    b. The gate drive will shut down when CS + RAMP > Comp.

    Regards,

    Mike