Hello,
i want to use the ucc28180 controller for my pfc. The informations About the PFC are:
-Vin= 90-130 VAC at 330-800Hz
-Vin_nrom= 115 VAC at 330-800Hz
f_sw = 250kHz
Vout= 350V
Pout= 105W
For the design i used the desing calculator and tested it on the UCC28180EVM-573. The IC works but the PF is not very well.
So my Problem is to improve the PF at low load. I measure a PF at about 20 W of 0.66 and at 50W of 0.88. The target is a PF of 0.95 at 50W and a higher PF at 20W.
The only difference to the calculations is, i used a Little bit higher inductor value.
So what can i Change to improve my PF.
Best regards