Dear all:
I have design the 4S2P LiFePO battery pack,the designed capacity is 7800mAh.I choose the Chem ID is 0438.the gg file is 7800mah.gg.zip,I do charge-discharge cycles, when discharge the battery pack,after FD is set,I found the FCC jumped from 6898mAh to 7569mAh.after charge the battery pack,FC is set,I found the FCC jumped from 7569mAh to 6862mAh.the log file is discharge-charge log.zip.why the FCC jump is so big?What factors determine the change?