Other Parts Discussed in Thread: TPS65279, DAC124S085, TLV9004, , TPS7A05
I have a high-power 6V-18V power source, and will be knocking it down to 5V with a TI TPS65279, which will introduce a ripple at 500kHz (which I will endeavor to filter some, but a significant 500kHz ripple will certainly remain). From this high-power 5V line, I want to generate a clean low-power 3.3V line, for driving an MSP432P401R, including associated ADC and DAC circuits (using a DAC124S085 and a TLV9004). Is the LM3281 a good choice for doing this?
If I filter out the 6MHz ripple as suggested by the inductor/capacitor choice in the LM3281 datasheet, can I also assume the the remaining 500kHz ripple (from the 5V line to which this component will be attached) will also be substantially reduced? Can this be quantified at all?
Thanks in advance for the help!