We have questions about TPS54302.
We want to change input voltage 24V to 8V or 8V to 24V.
Question 1.
Please tell us the recommended time that output voltage stabilizes by changing input voltage.
(We think that the IC needs waiting time until output voltage stability. )
Question 2.
Please tell us the minimum input voltage.
1. Vout=3.3V
2. Vout=5.0V
Question 3.
In datasheet p.13 Figure.15,
Plase tell us the allowable variation of R1~R5 value.
Plase tell us the allowable variation of C1~C5 value.
Can we use capacitor not recommended value about C1?
Must we use 22μF*2 about C4 and C5?
(Are there any problems about using 10μF*4 or 47μF*1?)
Can we use the capacitor anything other than 75pF about C6?
Question 4.
In datasheet p.17 Table.2,
Is C8 mistake in C6?
Best regards,
Takahiro Nishizawa