Other Parts Discussed in Thread: LM5066
Hello everyone,
I'm working on a board which has three indentical and independent LM5066i circuits (see attached circuit diagram). The dv/dt parts are assembled. All three circuits show the same effect described below.
The question is about the config resistor R271 on the PWR-pin on the bottom right. As I understood the datasheet, the maximum power loss limit of the MOSFET can be configured with this resistor. Increasing the resistance also increases the possible current allowed during startup, e.g. with capacitive load, especially without the dv/dt circuit.
But I recognized that this resistor also seems to affect the maximum continuous current in any way, after the output has been turned on without load. The shown value of 22k is too low for the application, the output voltage is turned off with only ~3 A of load. ~ 100k are enough to output the desired 10A. But when adding 3 x 100uH serial to the load resistors, 100k only allow the connection of ~9 A before turning off the output. I used high power resistors as load that have been connected to the output, after it has been turned on without the connected load.
The question I'm asking myself is, how does this PWR-resistor R271 affect the possible continuous output current? I only found information to calculate the power loss, I guess during startup. But this cannot be used for the continuous operation, as the power loss in this case is much lower than the configured value.
Best regards,
Christian