Other Parts Discussed in Thread: BQ25600, BQ25898, BQ25601D
I need to implement a circuit with USB Vbus (5V from USB connector) and with the management of battery recharge.
I would like to use the bq25910, but I discovered that also the part bq25600 should be similar, with the battery temperature sensor management too.
Then there is the part bq25898, but this should be usefull with USB OTG bus.
My goal is to have a Li-Battery 1Cell with 2A (discharge current) and 1-2Ah.
I need to load this battery when the USB cable is connected. In this case the current from USB will charge the battery and will supply the system.
When the USB cable will not be connected the battery will supply the system.
Can you help me to understand what is the best? Looking at the bq25910 examples I see bq25910 as slave and bq25600 as master connected together.
I'm thinking that bq25600 alone could do what I need.
Can you confirm me?
Thanks a lot.
Best regards Edo.