Dear Support Team,
We are using this device as the wireless receiver in our project. The battery specifications for charging current is like this:
Cell surface temp.(Celsius) Charge current
10 - 25 375mA max
26 - 45 750mA max
I wonder if we could set the temperature T1 = 10, and T2 = 25, and T3=T4=45 please?
If yes, how could we configure the NTC resistors then?
Thank you very much in advance!
Best regards
Weinan