Hi Experts,
I could see there is power good indication only for all SMPS rails in TPS659039-Q1 datasheet. Similarly is there any indication for LDO rails monitoring which are generated by PMIC internally?
Thanks
Manoj.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
I could see there is power good indication only for all SMPS rails in TPS659039-Q1 datasheet. Similarly is there any indication for LDO rails monitoring which are generated by PMIC internally?
Thanks
Manoj.
Manoj,
The GPADC can monitor up to two rails. You would have to connect those rails to the GPADC pins. This is the only internal option. Otherwise, you will need supervisors if the LDO rails need to be monitored.
Thanks,
Nastasha