Part Number: TPS7A7300
Customer is using TPS7A7300 to power a cell modem. The VDD_CELL rail has 2 x 100uF 1210 package ceramic capacitors. These are big ceramics (GRM32ER61A107ME20L). What should the feed-forward capacitor value be? The data sheet states "For output capacitors from 47 μF to 200 μF a feed-forward capacitor of at least 220 pF must be used." Customer is using a 1 uF Cff.
They are having an issue that the current draw of the cell modem through the TPS7A7300 is pulling down the 5V rail and causing processor reset or lock-up.
Any design suggestions here? I can send schematics via email.
Thanks,
Mark