Hi,
We are designing 2 buck regulators for our project, specifications for which are as below:
1) I/P V: 15V to 26V, O/P V: 12V, O/P I: 1.2A
2) I/P V: 15V to 26V, O/P V: 5V, O/P I: 1.0A.
Currently we are using 33uH inductor and 2*22uF/25V,1210,X7R capacitors.
We wanted to replace these ceramic capacitors with polymer caps eg: EEHZC1V470P or HHXA350ARA470MF61G
a. Can we replace ceramic capacitors directly with polymer caps?
b. Effect on stability of feedback loop?
c. Addition of 1uF/10uF ceramic capacitor in parallel to polymer capacitor. Will it help?