Hi all
Would you mind if we ask TPS1H000-Q1?
Our customer uses TPS1H000-Q1 with follow condtions;
-Vin=24V
-Iout=0.65A(this is the value which the customer would like to limit.)
-CL resistor(current limit resistor) = 750ohm ± 1%
They calculated RCL value using "RCL=VCL×KCL / 0.65A".
And then, they measured limit level.
The result was 750mA.
Even though it contains tolerace of resistor(±1%) and current accuracy(±10%), we assume that maximum current limit will be 711mA.
So, we would like to the difference between customer's calculation value and measurement result.
Could you let us know follows;
<Question1>
We would like to know external current limit accuracy correctly.
So, dose it mean followings?
①0.05≦Ilimit≦0.15@Vvs-Vout≦2.5V:±20%
②0.15≦Ilimit≦0.30@Vvs-Vout≦2.5V:±15%
③0.30≦Ilimit≦1@Vvs-Vout≦2.5V :±10%
Is it correct? And in case of customer's configuration, will the tolerance be pattern ③?
<Question2>
In relation to <Question1>, there is formula "RCL=VCL×KCL / Iout" on the datasheet P11.
VCL and KCL show only typical value.
So, we assume that the tolerance might be ±20% nevertheless of Ilimit.
<Question3>
There is the description of Isc(Short-circuit current limit), could you let us know it?
Is operating condition Vout=0?
Kind regards,
Hirotaka Matsumoto