This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601D: Maximum Output current

Part Number: BQ25601D
Other Parts Discussed in Thread: BQ25601

Hi

Myself I am a hardware engineer making a IoT device which has a specifications as listed below :

1. Li-Po battery of 3000 mAh

2. Battery Charging current 3 A

3. Maximum current required for the system (Maximum current through SYS pin) 3.5 A

I had gone through the datasheet of BQ25601D but I saw the maximum output current (through SW pin) as 3.25 A and The graphs are showing the Isys is upto 4 A.

Will the BQ25601D support a maximum Output current of 3.5 A?