Other Parts Discussed in Thread: AM5718, AM5728
Hi,
I want to have a battery to backup the RTC in TPS659037. Is that possible and how can that be done?
BR
Johan Bendz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a system with TPS659037 and AM5718 and I could use the RTC in any of these.
I will control the power on/off with the GPIO7 pin of TPS659037, could I configure a mode to just feed the PMIC RTC in this condition or could I configure to enable only LDO9 and use the RTC in AM5728 instead?
What would be the easiest way if I want to backup the RTC with a coin cell?
BR
Johan Bendz
Johan,
There is not a mode with just the PMIC RTC or just LDO9. The only way to use a back up battery would be to add a supervisor on VCC1 and turn on the backup when the main supply is too low. Unfortunately, this would not work well for a coin cell battery since the current consumption would drain the battery pretty fast.
Thanks,
Nastasha