This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS84A20: Possible maximum Peak Reflow Case temperature.

Part Number: TPS84A20

Hi Arrigo

The maximum possible Dwell time is 50 seconds at Peak reflow temp(245℃).

See Below Link.

e2e.ti.com/.../2682146

Then Is it possible to Dwell time from 250℃ to 20 seconds?

What is the maximum Dwell time at 250℃?

This device is only 245℃ for Peak reflow temp.

Regards.