Hi team,
Q1: I will use CSD22205L. But I cannot find the CAD fiel (.bxl) on the website. Would you send me the same package CAD file to me?
If you cannot provide the CAD file, I would like to get what the meaning for "7.2 Land Pattern Recommendation" and "7.3 Stencil Recommendation" in the datasheet.
If I design the package of this device, do I refer to the size of "7.2 Land Pattern Recommendation" or "7.3 Stencil Recommendation"?
Q2: 2 pin and 4 pin are all Drain. Are the two pins connected inside of the device? Do I still need to connect the two pins together in my circuit?