Other Parts Discussed in Thread: TLC59116
Dear Team,
My customer is using LP5018 for their design.
What is the difference between Maximum sink current and sink current limit?
They want to use OUT0-2 to control 9 LED.
They use 5V and 1 LED will consume around 10mA.
So the worst case will be 9 LED's(9*10mA) RGB current go to the maximum at the same time.
Which spec. should I follow?
If LP5018 is not suitable for this design, which components should I suggest to the customer?
Is TLC59116 or anything else?
Best Regards
Kevin