Hi TI,
We have one requirement:
DC-DC requirement:
1:Input voltage :0.5V-2.5V.
2:Output voltage :>3.8V(adj)
3:output current: >1A
could you please recommand one solution
thanks
peiyuanqing
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Peiyuanqing,
We have TPS61021A which can work with 0.5V-2.5V input voltage range and is capable of outputting 3.8V/1A from 1.8V. Do you want the device to output 1A from the input voltage down to 0.5V?. If the answer is yes, you need a much higher power boost converter like TPS61088. We have such a reference design. Please see TI reference design http://www.ti.com/tool/PMP9772.
best regards,
Gavin
Hi peiyuanqing,
Thanks for choose the TI solution. Here're my review result:
1. Please choose a >=10A current rating inductor. because at Vin=0.7V, Vo=3.8V, Io=1.3A condition, the average inductor current will be around 9A. And the input current will higher than 10A@ Vin=0.5V, Vo=3.8V/1A condition;
2. what is your lowest input voltage? if Vinmin=0.5V, then you have to choose TPS61200 instead of TLV61220. if Vinmin>=0.7V, then TLV61220 will be a better solution.