This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: Inverting converter is not regulating under load

Part Number: TPS65131

Hi,

     I'm also facing similar issue that TPS65131 not regulating under loaded condition for load of more than 20mA. The schematic looks fine matches with the datasheet. Now I have added a series resistor 100K with feed forward capacitor on negative side. The voltage output is set for +/-15V .VPOS is perfect and VNEG seems normal under no load condition. But when VNEG is loaded with 20mA load, It's output goes low as -17V.  Is there anything I'm missing?