This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: EN pin function for TPS61099

Part Number: TPS61099

Hi team,

 I would like to get the EN pin function of TPS61099.

Q1:If EN pin is low level, is the output voltage 0V? If the output voltage is not 0V, how much is the output voltage at this status?

Q2: The datasheet shows"When the EN pin is pulled to low voltage, the TPS61099x goes into shutdown mode." What is the shutdown mode?

Q3: I want to control the  TPS61099.  How can I control the device? Use a MOSFET on the IN pin?