Hello,
I am working on bq33100 and in this I need to configure the dataflash values.
For the faults like Overcurrent During Discharging (OC Dsg) there are Voltage Threshold values which need to be configured.
Consider the parameter : OC Dsg, in the description of this parameter they have set voltage thresholds, but to configure OC Dsg, we need current value.
According to our understanding, we can calculate the OC Dsg current value using the formula:
I = V/R
In our case
R: Current Shunt Register - 0.2mOhm
V: Voltage Threshold value from table
Is this understanding correct? If no, can somebody please explain the right procedure to follow?
What is the significance of RSNS ? For better accuracy of threshold configuration?
Can the same procedure be followed to calculate SC Dsg Cfg and SC Chg Cfg parameters?