Other Parts Discussed in Thread: TIDA-00173, UC3842, UCC28720, UCC28722, UCC28740, UCC28700
Dear sirs,
I´m involved in a new design including UCC28711. My design is a DC-DC flyback:
Input: 500VDC to 1300VDC
Output: 24vdc/0,2A (5W), Fmax= 80khz, eff=0,85
I am using the TIDA-00173 as a calculation reference.So the calculations are as follows:
DMAX = 1-DMAG-fmax * (Tr/2) . With fmax of 80khz, Dmax=0,5
Lpm = (2*Pout/eff) / IPPK2*fmax. So Lpm= 90mH
Ippk = 2*pout/eff*Vinmin*Dmax = 26mA
My questions are:
1) Can I use a much lower Dmax (i.e. 0,1) in order to get a much lower primary inductance. Any drawbacks?
2) With so low primary peak current (26mA) are there any drawbacks for designing/working properly?
3) My sensing resistor must be high (> 20 ohms) in order to ger a decent sensing voltage to the ic. Is it ok?
4) Is it better/easier/reliable to design for a higher output power specification?
5) Is it better another controller/design, (UC3842...)?. I need isolated output, Please sugggest the most adequate controller
6) The circuit may be a Primary or a Secondary side regulation. Which is the best in this design?
Best regards
Jean