I am reading the datasheet of LP5024. I saw that the PWM can be adjusted for each LED. Can I adjust LED current through I2C command? I saw that there is Current Range Setting using external resistor Riret, to set the LED current Imax to 25.5mA or 35mA. (page 15). There is color control and brightness control registers that can be accessed through I2C interface. Does either color or brightness control adjust the LED current? Or both works with PWM parameters?
Thanks.
Jin