Hi Sir,
I plan to study TPS62260DRV under this condition.
VIN : 6V
VOUT : 3.3V
IOUT : 100uA to 500mA
Target Efficiency : over 50% at 100uA, over 90% at 500mA
Mode pin : fixed Low (power save mode)
In this case this device behaves automatic transition from PFM to FPWM or vice versa.
My question is How much current is needed to change these mode?
Device datasheet (Page8) describes the picture of automatic mode transition but there is no current value in it.
Regards,