This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84824: soldering problem for TPSM84824

Part Number: TPSM84824

Hi, 

May I ask if there are anything need to be careful during soldering of TPSM84824? 

is there any concern for this kind of power module using hand soldering ?

Will there be any problem during rework? 

Thanks for your help.

  • When soldering any device, the max reflow and recommended solder profile must be observed.

    Hand soldering and rework is possible, but care must be taken to ensure all pins and pads are heated uniformally.

    Some details can be found in app-note: snva738