This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 OTG port is not working when powering up with AC charger connected

Other Parts Discussed in Thread: TPS65930, OMAP3530

Hello,

I'm running a custom board with OMAP3530+TPS65930+BSP6.14.01.

I followed below post @ http://e2e.ti.com/support/power_management/pmu/f/43/t/824.aspx to differentiate the AC charger and a USB PC connection. It's working now and I can achieve  a 1A charging with AC charger and 0.5A for PC USB.

However, when I connect the charger or USB to the board, and let the board power up into WINCE. The OTG port is not functioning.  If I power up the board 1st then connect the charger, the board works fine with HOST or DEVICE or AC charger.

I compared the ULPI registers and found no difference and now I can't find a way to solve the problem. Appreciate if anyone experience semilar problem can share your solution.

 

Thanks and best regards

Luo Yang