This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A85: Thermal resistance value

Part Number: TPS7A85


The thermal resistance value of TPS7A85A is different from the value of TPS7A85.

Is this true? If it is yes, why is the value different?

Best Regards,
Kohei Sasaki

  • Hi Kohei,

    The thermal resistance between TPS7A85A and TPS7A85 are different. There are a variety of factors that impact the thermal performance of a device including leadframe, die size, die placement/orientation in the package, mold compound, and more. While the type of package has a large impact on thermals, due to the other factors, there can still be a large variation between two devices in the same package.

    Very Respectfully,
    Ryan