This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS544C20: About detection method of PGOOD

Part Number: TPS544C20


Hi,

I understand that the PGOOD signal judges only depending on whether the FB voltage exceeds the threshold of PGH or PGL, is it correct?
If Yes, how long does it take from detecting the FB voltage to invert the PGOOD signal (H→L, L→H)?

Best regards,
Yuto Sakai

  • Sakai-san,
    There is no delay once the FB voltage crosses the limits. There is hysteresis based on voltage levels but no time delay once it is detected.

    Regards,
    Mathew
  • Hi Mathew-san,

    Thank you for your reply.
    What about the first line of the first post?
    >I understand that the PGOOD signal judges only depending on whether the FB voltage exceeds the threshold of PGH or PGL, is it correct?

    For example, in the case of OC or OT, does the PGOOD signal level invert at the moment of protection of OC and OT?
    Or does the PGOOD signal level be inverted when the output is stopped by OC or OT and the FB voltage is decreased to below the PGL threshold?

    Best regards,
    Yuto Sakai
  • Hi,

    PG can also be affected by OCP, EN signal and soft start done signal. If you are using some sort of AVS control on FB pin please filter it due to fast rise times can cause false tripping.

    Regards,
    Mathew
  • Hi Mathew-san,

    Sorry if it was not enough.
    Please let me organize the trip conditions of PG.
    Is the condition that PG inverts during normal operation only when the FB voltage exceeds the threshold (PGH, PGL)?

    Best regards,
    Yuto Sakai

  • Sakai-san,

    Yes during normal study state condition PG can go low only if the FB voltages crosses the thresholds for PGH and PGL.  If you have a PG glitch during normal operation in steady state please put inductor current probe and see if any OCP condition is not being caused.

    Regards,

    Mathew

  • Hi Mathew-san,

    Thank you for your reply.
    Datasheet P.5 In the description of the PGOOD pin, "Any fault condition causes this pin to pull low. "
    I understand that the FB voltage crosses the threshold value (PGH, PGL) by protection operation at all fault detections and the PGOOD signal goes low , is it correct?

    I am concerned whether the PGOOD signal may go low by only detecting the fault condition regardless of the FB voltage.

    Best regards,
    Yuto Sakai
  • Sakai-san,

    The datasheet is accurate and PG can go low when triggered by a internal fault condition such as OCP regardless of FB voltage. However in actual use case I don't think these are mutually exclusive events since OCP causes switching to turn off and output falls etc. However in the case of over voltage or undervoltage condition the PG acts first since the OVP and UVP thresholds are above and lower than PG thresholds.

    Regards,

    Mathew