This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25117: Lm25117 5v 10, D1 change, q1 shorted

Part Number: LM25117

We are using a 5V 10A power supply with the integrated LM25117, in one product. I attached the schematic
In the first production we use according to the plane D1 = PMEG6010CEH, the source worked very well.
In the second production due to lack of stock we use D1 = CDBMT160-HF.

of 6 power supplies that we tested, two put Q1 in short circuit, after approximately 10 minutes of operation, and with a load up to 500mA
Is it possible that the change of D1 produces this type of failure?