This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR16010: Rfbb and Rfbt not shown as 0402 package in the webench tool

Part Number: LMR16010


Tool/software: WEBENCH® Design Tools

Design specs: 48V in / 24V out / 1A

Why are Rfbb and Rfbt not shown in 0402 packages?

The webench tool show values of:

620k (Rfbt with package 0603 ...  1206)

20k (Rfbb with package 0805 ... 2010)

Is there a specific reason why 0402 resistors are not suggested?