Figure 23 in the datasheet shows an example where the battery is directly connected to the system. It explains that it is for 1-cell applications. The benefit is that the battery can automatically supplement the system load if the adapter is overloaded.
My question is if you can use this same configuration for a 3-cell application as well. Being able to supplement from the battery during high system loading is important to the design. If it is possible, is there anything that needs to change in Figure 23 besides the ISET, OVPSET, and FB pins? And what is the recommended value for the resistor between VREF and ACSET?
Thanks,
Kevin