This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630: Use with NCR18650B Li-Ion Cells

Part Number: BQ24630


Team,

My customer is looking for a charger for a 2s NCR18650B pack charged from a 12V input. Charge current is 1.6A and they need to avoid buck fsw at the AM frequency band. Could they use the bq24630? It is a Lithium Phosphate charger but looking at the charge profile I can't think of a reason why it wouldn't work. Would there be any trade-offs?

Thanks,

Antonio

  • Antonio,

    It is ok to use BQ24630 as long as following the design and layout guidelines described on the d/s and EVM User’s guide.

    Thanks,

    Ning.
    Please click "This Resolved my issue" button if this post answer your question.