This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS28225: Help to check internal resistor between pin4 and pin5.

Part Number: TPS28225


Hi Team,

My customer would like to understand the resistor value between pin4/pin5. They found the value seems varying a lot and concern if there could be potential issue. Thanks 

  • Hi Helios,

    Thanks for your field support. My name is Mamadou Diallo, I will help address your concerns.

    What values are your customers measuring? What do you mean by "varying a lot"?

    Thanks in advance for providing those details.

    Regards,

    -Mamadou
  • Hi Helios,

    Since I haven't heard from you in a while, I must assume that your problem was resolved and close this thread. If so, I would appreciate you sharing how your problem was resolved for others to benefit/learn from and also pressing the green button if in fact your problem was resolved.

    But if you're still having issues, please let us know and we will happily assist you in figuring out what is wrong.

    Thanks.

    Regards,

    -Mamadou
  • Hi Mamadou,
    This is Duncan for Quanta EE RD.

    This problem occurs at flying probe test in the production process of our products.
    The flying probe will measure the external resistor (100k ohm) on pin5 (LGATE) through ground.
    The measured value of most boards is 100K ohm, but only one PCBA is 23.34K ohm.
    TI also helped analyze (V-I curve) the IC, and the result is no problem.
    So we guess that there should be resistance to ground inside LGATE, and What is the resistance value?
    And should we modify our measurement specifications?

    BR
    Duncan
  • Suggest as Answer
  • Hi Duncan,

    Glad to hear back from you. Which datasheet did you find that block diagram attached on your first post?

    It seems odd since I am looking at TPS28225's datasheet and as you can see below, we do not specify a resistor between pin 4 and pin 5 and even more puzzling is the fact that you're measuring a 100kohm resistance between the 2 pins. 

    The picture below is from the following link:

    www.ti.com/.../tps28225.pdf

      But that resistor would only be there to prevent any open-gate conditions and any accidental turn on during output active low events on the power FET. 

    It can also be set externally by simply connecting the desired resistance value from pin 5 to ground.

    What application and in what topology are they using the device that the customer is concerned?

    Thanks.

    Regards,

  • Hi Mamadou,
    Sorry, the part number we use is TPS28225-Q1 (for automotive), Not TPS28225 (for consumer).
    datasheet link : www.ti.com/.../tps28225-q1.pdf
    thanks
  • Hi Duncan,

    Thanks for clarifying that. I don't believe there is any need to modify any measurements specifications.

    How many devices did they test that resulted in the resistor being 100 kohm.
    Is the customer not sure whether the actual value should be 100 kohm?
    I would suspect the 23.34 kohm reading from the one device to be an off/error.

    I will order samples which takes about 2-3 business days to ship and measure on the bench and I will get back to you by COB next week on Thursday (Dallas time).

    Thanks for your patience.

    Regards,

    -Mamadou
  • Hi Duncan,

    Thanks for your patience!

    After bench characterization of ordered samples at room temperature, I measured resistance between LGATE and GND to be 240.6k 240.1k 243.8k 244.2k.

    Also to consider is the fact that resistors in our process typically vary by +/-20%.

    Can you please verify your measurements again just to make sure?

    Thanks for your time.

    Regards,

    -Mamadou
  • Hi Mamadou,

    below list to show the resistance between the pin4 and pin5 of TPS28225-Q1.

    Sample1 (call "NG sample"):

    The resistance is 85.7K.

    Sample2 (call "NG sample"):

    The resistance is 270K.

    Sample3 (call "Good sample")

    The resistance is 1.8M.

    And please help to the difference on the marking.

    1. NG sample : PXND TI 75K 0708

    2. Good sample : PXND TI 6CK AGHF

    thanks

  • Hi Duncan,

    Thanks for getting back to me.

    Our local team will follow up with you this matter as soon as possible to get to the bottom of this issue.

    In the meantime, I will go ahead and close this thread.

    Thanks for your patience.

    Regards,

    -Mamadou