This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61177A: Is a pull-down recommended for the ENB input?

Part Number: TPS61177A

Hi Folks,

I'm designing in the TPS61177A chip and I have a question regarding the ENB input.  My microcontroller output doesn't have the option of enabling a pull-down (only pull-up) so do you recommend putting a pull-down resistor on the ENB line?  Will I still need the 10K resistor in series with the ENB input?

Thanks in advance,

Richard