This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170: Charging Current Issue

Part Number: BQ24170


I am facing problem in BQ24170 Charger IC following

1. If Input Voltage rises from 12V to 15Volt , the charging current also increases. Charging current not constant. 

2. While charging the battery , if load is connected (2A) suddenly... the status LED starts blinking, but Battery is charging (charge Current decreased ,System Out Current Increased)

My Design Specs:-

1. Input Adopter 12.5V/5A.

2. Li-Ion 3.7 Volt/10A- Battery-3 in Series.

0878.Battery Charger.pdf