Hello,
This is my first attempt at a solder mask defined package, as I could not find an existing LMZM power module package in the eaglecad TI libraries. I have attached the land pattern supplied by the data sheet and also the package file i've been working on (see link below). It is not completed but was wondering if the negative solder mask (white) has been done correctly thus far for the pads, as from my understanding there is metal under soldermask for all the pads on this footprint. I'm also curious as to any existing packages for this power module in other pcb s/w (e.g. Kicad). I've centered the coordinate system to the package outline and based each of the pads on the coordinates in the land pattern.
Your help is greatly appreciated.
/cfs-file/__key/communityserver-discussions-components-files/196/2045.lmzm33603.zip